Installation Instructions for PEx i.MX 6UltraLite v1.1 Service Pack Eclipse Update


1. Download 'PEx_i.MX_6UL_v1.1_ServicePack_Eclipse_Update_b160317.zip' archive package

2. Run your Eclipse IDE

3. Go to Help >> Install New Software... >> Add...

4. Fill the name of the new software site, for example 'PEx i.MX 6UL v1.1'

5. Select Archive... and find the downloaded archive package

6. Select the 'Processor Expert for i.MX 6UL Eclipse Update' group of items to be installed

7. Follow the guided installation process

8. Eclipse will ask you to restart the environment as the last step of the installation process. Please do so.

9. After restarting the Processor Expert refresh the installed data and content of the Service Pack for the i.MX 6UL processors

10. You can start using the tool and work with i.MX 6UL v1.1




  Known Problems and Limitations


 - None.


  Revision history

  Changes in device support since the 1.1.0 Alpha version, January 29th 2016

 - Updated list of part numbers for 6UL v1.1 processors according to current datasheets information:

   * CPUs - iMX 6UltraLite in 14x14 package

    - MCIMX6G3DVM05AA, MCIMX6G3CVM05AA
    - MCIMX6G2DVM05AA, MCIMX6G2CVM05AA, MCIMX6G2AVM05AA, MCIMX6G2AVM07AA
    - MCIMX6G1CVM05AA, MCIMX6G1AVM05AA, MCIMX6G1CVM07AA
    - MCIMX6G0DVM05AA

   * CPUs - iMX 6UltraLite in 9x9 package

    - MCIMX6G3DVK05AA, MCIMX6G3CVK05AA
    - MCIMX6G2DVK05AA, MCIMX6G2CVK05AA

 - Fixed 9x9 package supply pins location of [K6] NVCC_DRAM_2P5 and [N6] NVCC_DRAM.


  Changes in device support since the 1.0.0 version, December 9th 2015

 - Support of device changes based on the last datasheets and RM Rev 0 draft B, 01/2016; Only the content 
   of peripheral registers has been updated in 6UL processor database files and SDK header file, 
   no IOMUXC functional changes since the Service Pack Update (REV 2) 12/9/2015


  Changes in device support since the 1.0.0 version, September 14th 2015

 - Updated part number identification using fully qualified part name.
 - Updated feature support for "G0" and "G1" devices - fixed UART, ENET, USB, LCDIF, QSPI, SDIO, ISO7816-3, SPI, Timers and ADC peripheral signals.


  Changes in device support since the alpha version, June 17th 2015

 - Support of ADC peripherals has been added in Release Candidate 1
 - Support of device changes based on the last datasheet and RM Rev.0, 08/2015.
 - Fixed initialization of 'SELECT_INPUT' registers involved in daisy chaining of some input pad signals.



http://www.freescale.com/peximx
http://www.freescale.com

Freescale Support Department:
 support@freescale.com